AXIS#.SENSORLESS.ENPHASELEAD

Description

When the motor electrical frequency gets close to the bandwidth of the sensorless algorithm, the phase lag in the estimated commutation angle increases. This can increase the required voltage and current to produce the same amount of torque. A phase lead compensator is added to the sensorless algorithm to address this. This phase lead compensator eliminates the phase lag in all velocities no matter the bandwidth. Enable this feature by setting AXIS#.SENSORLESS.ENPHASELEAD to 1.

Versions

Action Version Notes
Implemented 02-03-03-000

 

General Information

Type

Read/Write

Description Enables/disables phase lead compensation

Units

N/A

Range 0 to 1
Default Value 0

Data Type

Boolean
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
AXIS1.SENSORLESS.ENPHASELEAD

5018h

02h

Unsigned8

-

-

Read/Write

No

AXIS2.SENSORLESS.ENPHASELEAD

5118h

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.SENSORLESS.ENPHASELEAD

7406

1CEE

Unsigned8

Read/Write

-

AXIS2.SENSORLESS.ENPHASELEAD

72942

11CE

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SENSORLESS.ENPHASELEAD

7406

Unsigned8

Read/Write

-